programmable pins of MC68HC908QB8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

programmable pins of MC68HC908QB8

3,109 Views
abhi_roy03
Contributor I
Hello
I am using MC68HC908QB8 microcontroller in my project.Can i connect port A of the microcontroller to the programmer.The microcontroller has 16 pins in total.It has 6 pins which are dedicated for multiple purposes(I/O port,A/D channel,Key board interface bits).if notkindly update me on the programmable pins of the QB8 microcontroller.
 
regards
Abhishek
Labels (1)
0 Kudos
Reply
2 Replies

784 Views
RaghuSorab
Contributor I

Hi Abhishek,

To the best of my knowledge, all the QT Devices have the PTA0 as the COM, PTA4 is tied to ground and PTA1 is tied to VCC.

It is the MON08 standard. Please do refer the programmer manual in which the MON08 pinouts for the specific Device will be given.

Hope this makes it clear.

Raghu Sorab

 

 

 

0 Kudos
Reply

784 Views
peg
Senior Contributor IV

Hi Abhishek,

I am not sure what you are asking...

The MON08 pins of this device are all on Port A already.

All MON08 functions are tied to a particular pin, you cannot change this!

Maybe try to rephrase your enquiry.

Regards David

 

0 Kudos
Reply