problems burning 908GP32CPE using PROG08sz and ICS08

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

problems burning 908GP32CPE using PROG08sz and ICS08

33,822件の閲覧回数
kitoff
Contributor I
Hi,
 
I am using PROG08SZ software and ICS08 dev. board to program GP32CPE chips.
After passing all the security bits successfully and choosing the .08P file as 908_GP32_highspeed.08P, the following words appears:"Error writing block data to part.Disabling block write". Then the PROG08SZ software is too slow to reply any action that I click the mouse, so I have to use ctrl+alt+del and then kill this procedure.
 
Meantime, I use this software+hardware to program 908JL16 and LJ24 chips, everything is OK.
 
In CW5.1 for HC08 the same problem and indication appears.
 
Please help me, I do not know where is mistake.
 
snapshot of the error massege is attacked here below.
 
Thanks a lot.
 
Message Edited by t.dowe on 2009-09-04 02:24 PM
ラベル(1)
0 件の賞賛
返信
25 返答(返信)

3,333件の閲覧回数
peg
Senior Contributor IV
Hi FOLSOT,
 
Did you get this comment verbatim from Freescale?
 
I believe this is comments made by John Hartman of NoICE.
 
0 件の賞賛
返信

3,330件の閲覧回数
kitoff
Contributor I
Hi, all
 
I have to thank you all for any help.
 
To Ablan, I am sorry about this thing too, but it's up to the decison of my boss and I can't force him to change his determination. In fact I love freescale's chips and I still use them personally, but of course not GP32, this never works for me and I fell my head hot when touching is now,hehe.
BTW, your chinese is pretty good and I hope I can invite you to have a cup of chinese tea someday in China:smileytongue:.
 
To Peg, I am using real com port, definitely! I am not talking problems of USB-COM convertors. Up to now never worked well with GP32+mon08.
 
To Maraja, I tried your instruction and failed, maybe you are using a pcmia card and I don't have one that.
 
To Alegna, I will try that you suggust. Thanks a lot.
 
To Mark, your replies are always late and bad. The same to your service. The only thing I can do is never considering any PE products, as I did now. 
 SO SORRY FOR YOUR POOR Service.

To FOLSOT, I also read the issue from noice website. USB convertors with PL2303 chips are not working with the SW+laptop. I have a convertor HP OEM convertor with FDTI chip and works fine for all 08s except for GP32.


 
 
 


Message Edited by kitoff on 2007-06-14 02:25 AM

Message Edited by kitoff on 2007-06-14 02:26 AM
0 件の賞賛
返信

1,729件の閲覧回数
peg
Senior Contributor IV
Hi kitoff,
 
I have been using the high speed version for GP32 version 1.03 .08p file (as you seem to be) for a long time now and never had any trouble whatsoever (with hundreds of devices).
Have you tried the non-high speed version? Perhaps your hardware does not handle the high speed one properly.
 

Message Edited by peg on 2007-05-0207:43 AM

0 件の賞賛
返信

1,729件の閲覧回数
Maraja
Contributor I
Hi,
 
I had the same problem when try program using a BBL PCMCIA Card adapter for RS232. After changes many parameters I found the one that make load algorithm successfully done.
 
Maybe the FIFO receiver parameter should by 1 for other adapters and hard RS232 too. To found where's the parameter try see hardware guide's or on Manage device on Ruindows®. In my case deactive FIFO isn't enough, first I need to set receiver with "1".
 
Best regards,
Marajá
 
 
Message Edited by t.dowe on 2009-09-04 01:59 PM
0 件の賞賛
返信

1,729件の閲覧回数
peg
Senior Contributor IV
Hi,
 
All of my computers have "real" serial ports and I always just use the default FIFO setting of 14 on recieve and 16 on transmit without any issues.
I have tested two converters and found that they did not work with MON08 adapters but never got to the bottom of it as I don't have to....... yet. Field service notebook PC needs replacing soon. Two problems here, have they a serial port and all the good deals come with Vista!
 
0 件の賞賛
返信