on delay

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

on delay

1,851 次查看
jakjeon2
Contributor I

Off Delay type changed to on delay type.

Dear sir,

Attach relay control part source.

The current relay time delay is an OFF DELAY type. We want to change this to ON DELAY type.

That is, it is necessary to change the output to "on" after a certain time after the input is turned on. There are no conditions (people, tools, etc.) to do this, and we ask for support(help).

It is really urgent.

In addition, the entire program source is attached. Please refer.

Device is MC68HC705.

This is a program made in motorola assembly language.

I will be waiting for your quick reply.

0 项奖励
回复
2 回复数

1,725 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

I am not good in ASM code and this is very old, but I am not sure that the code is complete.

regards

0 项奖励
回复

1,725 次查看
tonyp
Senior Contributor II

This is certainly not a complete program.  It lacks a whole bunch of symbol definitions, a reset vector, proper initialization, etc.

0 项奖励
回复