on delay

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

on delay

1,846 Views
jakjeon2
Contributor I

Off Delay type changed to on delay type.

Dear sir,

Attach relay control part source.

The current relay time delay is an OFF DELAY type. We want to change this to ON DELAY type.

That is, it is necessary to change the output to "on" after a certain time after the input is turned on. There are no conditions (people, tools, etc.) to do this, and we ask for support(help).

It is really urgent.

In addition, the entire program source is attached. Please refer.

Device is MC68HC705.

This is a program made in motorola assembly language.

I will be waiting for your quick reply.

0 Kudos
Reply
2 Replies

1,720 Views
vicentegomez
NXP TechSupport
NXP TechSupport

I am not good in ASM code and this is very old, but I am not sure that the code is complete.

regards

0 Kudos
Reply

1,720 Views
tonyp
Senior Contributor II

This is certainly not a complete program.  It lacks a whole bunch of symbol definitions, a reset vector, proper initialization, etc.

0 Kudos
Reply