kl03 Output short circuit to ground

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

kl03 Output short circuit to ground

1,573 次查看
DieterK
Contributor I

Can a MKL03Z8VFG4 GPIO configured as an Output and driven high be destroyed, when it is shortened to Vss over a long period of time?

0 项奖励
回复
1 回复

1,466 次查看
john_suchyta
NXP Employee
NXP Employee

Yes. The short to ground will exceed the 25mA max current spec for the output pin. This will cause localized heating on the die which will affect the reliability and lifetime of the chip.

Regards,

John

0 项奖励
回复