kl03 Output short circuit to ground

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

kl03 Output short circuit to ground

1,574件の閲覧回数
DieterK
Contributor I

Can a MKL03Z8VFG4 GPIO configured as an Output and driven high be destroyed, when it is shortened to Vss over a long period of time?

0 件の賞賛
返信
1 返信

1,467件の閲覧回数
john_suchyta
NXP Employee
NXP Employee

Yes. The short to ground will exceed the 25mA max current spec for the output pin. This will cause localized heating on the die which will affect the reliability and lifetime of the chip.

Regards,

John

0 件の賞賛
返信