kl03 Output short circuit to ground

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

kl03 Output short circuit to ground

1,033 Views
DieterK
Contributor I

Can a MKL03Z8VFG4 GPIO configured as an Output and driven high be destroyed, when it is shortened to Vss over a long period of time?

0 Kudos
Reply
1 Reply

926 Views
john_suchyta
NXP Employee
NXP Employee

Yes. The short to ground will exceed the 25mA max current spec for the output pin. This will cause localized heating on the die which will affect the reliability and lifetime of the chip.

Regards,

John

0 Kudos
Reply