included S19 file isn't updated when compiling

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

included S19 file isn't updated when compiling

Jump to solution
1,399 Views
Seppel
Contributor I

Hi @all,

 

in my application PRM file i include bootloader by HEXFILE ..\bin\bootloader.s19 instruction. If i do some small changes in this bootloader.s19 file (f.e. only one var value changed in bootloader project and became recompiled) and copy paste the new file in app folder, and than recompile the app -> the app still works with the old bootloader.s19 file. Compiler don't realizes that the bootloader.s19 file has changed a little bit, and don't refresh it.

 

How can i teach the compiler to compile the bootloader.s19 each time, by every compilation progress, unless it have changed or not?

Labels (1)
0 Kudos
Reply
1 Solution
1,213 Views
Ware
Contributor III

 

For original CodeWarrior

  1. Select: PROJECT->Remove Object Code
  2. Then recompile

 

For Eclipse-based CodeWarrior (v10+)

  1.  Select: PROJECT->Clean
  2. Then recompile

 

 Regards,

 - Ware

 

View solution in original post

0 Kudos
Reply
2 Replies
1,214 Views
Ware
Contributor III

 

For original CodeWarrior

  1. Select: PROJECT->Remove Object Code
  2. Then recompile

 

For Eclipse-based CodeWarrior (v10+)

  1.  Select: PROJECT->Clean
  2. Then recompile

 

 Regards,

 - Ware

 

0 Kudos
Reply
1,213 Views
Seppel
Contributor I

Thanks, just one click more i would like to have, but it works :smileywink:

0 Kudos
Reply