hi everyone.I need help.when I use MC9S08SG32.I want to use SCI  IDLE line wake up,but i cannot set the RWU bit to 1. why? and what is the correct method  to use the IDLE LINE wake up .which register need set.Thanks very much.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

hi everyone.I need help.when I use MC9S08SG32.I want to use SCI  IDLE line wake up,but i cannot set the RWU bit to 1. why? and what is the correct method  to use the IDLE LINE wake up .which register need set.Thanks very much.

507件の閲覧回数
zhaosen
Contributor I

hi everyone.I need help.when I use MC9S08SG32.I want to use SCI  IDLE line wake up,but i cannot set the RWU bit to 1. why? and what is the correct method  to use the IDLE LINE wake up .which register need set.Thanks very much.

 

!

ラベル(1)
0 件の賞賛
返信
0 返答(返信)