hi everyone.I need help.when I use MC9S08SG32.I want to use SCI  IDLE line wake up,but i cannot set the RWU bit to 1. why? and what is the correct method  to use the IDLE LINE wake up .which register need set.Thanks very much.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

hi everyone.I need help.when I use MC9S08SG32.I want to use SCI  IDLE line wake up,but i cannot set the RWU bit to 1. why? and what is the correct method  to use the IDLE LINE wake up .which register need set.Thanks very much.

532 Views
zhaosen
Contributor I

hi everyone.I need help.when I use MC9S08SG32.I want to use SCI  IDLE line wake up,but i cannot set the RWU bit to 1. why? and what is the correct method  to use the IDLE LINE wake up .which register need set.Thanks very much.

 

!

Labels (1)
0 Kudos
Reply
0 Replies