hi everyone.I need help.when I use MC9S08SG32.I want to use SCI  IDLE line wake up,but i cannot set the RWU bit to 1. why? and what is the correct method  to use the IDLE LINE wake up .which register need set.Thanks very much.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

hi everyone.I need help.when I use MC9S08SG32.I want to use SCI  IDLE line wake up,but i cannot set the RWU bit to 1. why? and what is the correct method  to use the IDLE LINE wake up .which register need set.Thanks very much.

508 次查看
zhaosen
Contributor I

hi everyone.I need help.when I use MC9S08SG32.I want to use SCI  IDLE line wake up,but i cannot set the RWU bit to 1. why? and what is the correct method  to use the IDLE LINE wake up .which register need set.Thanks very much.

 

!

标签 (1)
0 项奖励
回复
0 回复数