ethernet communication with PT60?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ethernet communication with PT60?

跳至解决方案
1,112 次查看
eliezeroc
Contributor III

Hello. I'm developing a project that requires Ethernet communication. My project is being developed with the PT60, then I have to use an external module for communication. Does anyone have any idea what kind of module should I use? Just remember that to be a low-cost project I can not use a Knets. Thank you.

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,015 次查看
tonyp
Senior Contributor II

Although I doubt an external module will be a cheaper overall solution, here's a couple of suggestions:

1. Have a look at Tibbo modules.  They have a large variety, and I've used several with mostly good results.  Some have only single socket capability so depending on your app you may want to stay away from them as the work-around for multiple connections becomes quite involved -- even though, the connections are not simultaneous.

2. Have a look at Wiznet (e.g., WZ5100) chips.  They are much more affordable (and I would even say, much more flexible) than Tibbo modules but with more work on your end.

Hope this helps.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,016 次查看
tonyp
Senior Contributor II

Although I doubt an external module will be a cheaper overall solution, here's a couple of suggestions:

1. Have a look at Tibbo modules.  They have a large variety, and I've used several with mostly good results.  Some have only single socket capability so depending on your app you may want to stay away from them as the work-around for multiple connections becomes quite involved -- even though, the connections are not simultaneous.

2. Have a look at Wiznet (e.g., WZ5100) chips.  They are much more affordable (and I would even say, much more flexible) than Tibbo modules but with more work on your end.

Hope this helps.

0 项奖励
回复
1,015 次查看
eliezeroc
Contributor III

Thank you, I will study your suggestion.

0 项奖励
回复