ethernet communication with PT60?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ethernet communication with PT60?

ソリューションへジャンプ
1,786件の閲覧回数
eliezeroc
Contributor III

Hello. I'm developing a project that requires Ethernet communication. My project is being developed with the PT60, then I have to use an external module for communication. Does anyone have any idea what kind of module should I use? Just remember that to be a low-cost project I can not use a Knets. Thank you.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,689件の閲覧回数
tonyp
Senior Contributor II

Although I doubt an external module will be a cheaper overall solution, here's a couple of suggestions:

1. Have a look at Tibbo modules.  They have a large variety, and I've used several with mostly good results.  Some have only single socket capability so depending on your app you may want to stay away from them as the work-around for multiple connections becomes quite involved -- even though, the connections are not simultaneous.

2. Have a look at Wiznet (e.g., WZ5100) chips.  They are much more affordable (and I would even say, much more flexible) than Tibbo modules but with more work on your end.

Hope this helps.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,690件の閲覧回数
tonyp
Senior Contributor II

Although I doubt an external module will be a cheaper overall solution, here's a couple of suggestions:

1. Have a look at Tibbo modules.  They have a large variety, and I've used several with mostly good results.  Some have only single socket capability so depending on your app you may want to stay away from them as the work-around for multiple connections becomes quite involved -- even though, the connections are not simultaneous.

2. Have a look at Wiznet (e.g., WZ5100) chips.  They are much more affordable (and I would even say, much more flexible) than Tibbo modules but with more work on your end.

Hope this helps.

0 件の賞賛
返信
1,689件の閲覧回数
eliezeroc
Contributor III

Thank you, I will study your suggestion.

0 件の賞賛
返信