addressing with SMAC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

addressing with SMAC?

1,619 Views
hdeweyh
Contributor I
Hello,
I am using MC13231-SRB and beekit and the SMAC protocol to setup some home-automation type of applications. My question is whether it is possible to do low level addressing using SMAC or if addressing must be done within the data of the sent packet and handled by the higher level code?

Thanks,
Heather
Labels (1)
0 Kudos
Reply
1 Reply

1,024 Views
addiyi
NXP Employee
NXP Employee
Hello Heather,

SMAC only implements the layer to handle the transceiver it means transmit, receive, change channel, adjust transmitter output power, CCA operation and low power modes. SMAC is intended to provide a communication point to point since it doesn’t implement any networking function like bind, associate, dissociate, addressing, etc. My advice is to use MAC codebase, witch all ready have implement network layer.

Regards,
Adrian
0 Kudos
Reply