addressing with SMAC?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

addressing with SMAC?

1,598件の閲覧回数
hdeweyh
Contributor I
Hello,
I am using MC13231-SRB and beekit and the SMAC protocol to setup some home-automation type of applications. My question is whether it is possible to do low level addressing using SMAC or if addressing must be done within the data of the sent packet and handled by the higher level code?

Thanks,
Heather
ラベル(1)
0 件の賞賛
返信
1 返信

1,003件の閲覧回数
addiyi
NXP Employee
NXP Employee
Hello Heather,

SMAC only implements the layer to handle the transceiver it means transmit, receive, change channel, adjust transmitter output power, CCA operation and low power modes. SMAC is intended to provide a communication point to point since it doesn’t implement any networking function like bind, associate, dissociate, addressing, etc. My advice is to use MAC codebase, witch all ready have implement network layer.

Regards,
Adrian
0 件の賞賛
返信