Zstar2 and 3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Zstar2 and 3

2,129 Views
hityou123
Contributor II
I am thinking of getting either zstar2 or zstar 3 demo board.
Whats the difference between them?
Zstar2 includes both the sensor and the wireless transceiver, correct?
Labels (1)
0 Kudos
Reply
1 Reply

1,171 Views
ok2ucx
Contributor IV
Hi,

all ZSTAR(1), ZSTAR2 and ZSTAR3 sensor boards do always have accelerometer sensor, MCU and the wireless transceiver. The only difference is that:

ZSTAR has MMA7260Q sensor, MC9S08QG8 MCU and MC1319x wireless chip

ZSTAR2 is almost identical, just different sensor used - MMA7360L

the latest development ZSTAR3 combined MCU + wireless MC1321x family chip
and the two options for the sensor:
  • MMA7361L analog or
  • MMA7456L digital  accelerometer

So far, just one type of the USB stick (with HC908JW32) is used to connect any of these sensors. RD3172MMA7456L_SW and accompanying firmware allow multiple sensors with one USB stick.

Pavel, Freescale Czech


Message Edited by ok2ucx on 2009-01-06 09:06 AM

Message Edited by ok2ucx on 2009-01-06 09:06 AM
0 Kudos
Reply