Zigbee/IEEE802.15.4   MC13192evb code development Asp_GetTimeReq(zbClock24_t *time)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Zigbee/IEEE802.15.4   MC13192evb code development Asp_GetTimeReq(zbClock24_t *time)

1,966件の閲覧回数
beedeveloper
Contributor I

Zigbee/IEEE802.15.4   MC13192evb code development

In the 802.15.4 MAC/PHY SoftwareReference Manual (802154MPSRM.pdf)

I read :

5.3.1void Asp_GetTimeReq(zbClock24_t *time)

This function requests the current value of the transceiver internal event timer.

The time pointer points to a 3 byte array where the value of the transceiver’s internal 24 bit event timer will be copied. The current value of the internal event timer (0x000000 to 0xFFFFFF) is a little endian byte array. The function does not return any value because the call is always successful.

What are the granularity and resolution of the current time returned with *time?

ラベル(1)
0 件の賞賛
返信
1 返信

1,013件の閲覧回数
Mads
Contributor V
Hi,
the Clock are setup to run based on the "symbol" time that 802.15.4 uses.
this is 16uSec per symbol.
 
e.g

5 second are:  5E-6 / 16 = 0x04c4be

BR,

Mads Westergreen

0 件の賞賛
返信