ZStar as Remote Mouse with Buttons

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ZStar as Remote Mouse with Buttons

1,907 Views
funutation
Contributor I
Hi

I am newbie.

I want to use my ZSTAR demo to take over control of the mouse of my computer so
that I can use it as a remote mouse with button presses enabled as well.

How can I do this?  The Triax software just works inside that window.  How do I get
it to become my remote mouse?

I see comments about demo software.  Where do I find this?
thanx
ted


Labels (1)
0 Kudos
Reply
1 Reply

1,090 Views
funutation
Contributor I
I might be getting warm...I got this from another location

Since the USB stick comes from the factory with two dualboot-aware applications pre-programmed, you can switch the ZSTAR demo board to work like a remote mouse easily by pressing the button on the USB stick. This information can be found in the ZSTAR Reference Manual (page 53):

http://www.freescale.com/files/sensors/doc/ref_manual/ZSTARRM.pdf

Movement of the cursor on screen is done very simply by tilting the sensor board in XY-axes. The two buttons on the Sensor board have the same functions as buttons on a real mouse.

Your game application is very interesting, I would recommend to try it. You can find more information on HID Class – Mouse in the AN3153 “Using the Full-Speed USB Module on MC68HC908JW32” on the web:

http://www.freescale.com/files/microcontrollers/doc/app_note/AN3153.pdf

0 Kudos
Reply