WinIDE Simulate PLL  HC08

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

WinIDE Simulate PLL  HC08

4,596 次查看
zen
Contributor I
HI, All
     I am a beginner to HC08 and ICS08GPGTZ. I wonder how to skip the below code
             BRCLR  6,PBWC,*
     in the ICS08GP  In-Circuit Simulator when I simulate the code without connecting board?
    
     I tried
               bset 6,PBWC
      But failed.
 
                               Thanks               Zen
标签 (1)
0 项奖励
回复
3 回复数

2,175 次查看
Zahar
Contributor IV
Zen,

There are a couple other ways that you can surpass this line of code during your simulation session.

After loading your code into P&E ICS08 full chip simulation you can:

1. Use PC 'name of sub-routine or location of code' to set your program counter to correct line.

2. You can right click your mouse pointing to a particular location and choose to set your Program Counter to the place where your mouse is pointing.

Best Regards,
Zahar
P&E
0 项奖励
回复

2,175 次查看
zen
Contributor I
Thanks Encoder,
    You introduced two approaches to the above simulation problem.  I will spend more time on the WinIDE tool.
                       zen
0 项奖励
回复

2,175 次查看
Encoder
Contributor I
BRCLR  6,PCB,*
 
is a conditional delay based on a bit test on PBWC which is the lock bit of the PLL register. It translates in a 3 byte line of code and in an undetermined delay.
 
I cannot say anything for the delay but the instruction may be replaced by
 
NOP
NOP
NOP
 
which is 3 bytes long and takes 3 HC08 clock cycles just making nothing else. I think that this is ok for your simulation. The best approach is anyway to skip this line by a semicolon to make an easy restoration when compiled on the real board:
 
; BRCLR  6,PCB,*
 
Encoder


Message Edited by Encoder on 2008-03-12 06:54 PM
0 项奖励
回复