Which Bootloader

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Which Bootloader

1,636 次查看
Yoheeb
Contributor I

Hi all.

 

I have managed to wedge my app inside the CMX gernic hid demo application.  WHile not the cleanest way to go, it was quick and dirty for what I needed.

 

My question now is, which bootloader do I wedge into it?  I have seen posts for both the AN3561 and the AN 2295.

 

Also, I am putting this in place backwards, since it would of been easier to create a project from scratch using either one as a template, so would either of these be easier to jam in?  or am I even asking the right question here?

 

I do need to program over USB, the host system is controlled, so we can make sure all appropriate drivers will be in place, it need not be a CDC-HID, it can be anything.  Also, invoking the bootloader by jumpering an input is fine, it isn't required to be invoked remotely, although I wouldn't discard that option if it were there.

 

Thanks in advance,

 

Sincerely,

 

Yoheeb

标签 (1)
0 项奖励
回复
1 回复

1,360 次查看
Yoheeb
Contributor I

I conviently failed to mention I am using an MC9S08JM60.  Sorry about that.  Working with the demoJM board at the moment.

0 项奖励
回复