What is the proper USB Driver for the TWR-S08LL64 Kit bdm debugging?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the proper USB Driver for the TWR-S08LL64 Kit bdm debugging?

690 Views
PG1
Contributor I

I cannot communicate with the board so I am wondering if the right USB driver got installed.

 

The debugger cable is simply a usb cable to a socket on the board--no bdm multilink necessary.

 

I let WindowsXP install the driver and it chose "Open Source BDM-JM60 (libusb-w32)".

Can anyone confirm that this is the correct driver?

 

 

I have already installed different drivers for an LL16 demo board and USB BDM MULTILINK.

Labels (1)
0 Kudos
Reply
1 Reply

576 Views
PG1
Contributor I

THe OSBDM driver is correct.

 

The problem is that the TWR_S08LL64 comes pre-programmed with an app that disables the debugger in a low power mode.

Pushing a button causes the app to wake up the CPU and get a clock to the debugger. Communication can then take place.

0 Kudos
Reply