What is the proper USB Driver for the TWR-S08LL64 Kit bdm debugging?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the proper USB Driver for the TWR-S08LL64 Kit bdm debugging?

1,081件の閲覧回数
PG1
Contributor I

I cannot communicate with the board so I am wondering if the right USB driver got installed.

 

The debugger cable is simply a usb cable to a socket on the board--no bdm multilink necessary.

 

I let WindowsXP install the driver and it chose "Open Source BDM-JM60 (libusb-w32)".

Can anyone confirm that this is the correct driver?

 

 

I have already installed different drivers for an LL16 demo board and USB BDM MULTILINK.

ラベル(1)
0 件の賞賛
返信
1 返信

967件の閲覧回数
PG1
Contributor I

THe OSBDM driver is correct.

 

The problem is that the TWR_S08LL64 comes pre-programmed with an app that disables the debugger in a low power mode.

Pushing a button causes the app to wake up the CPU and get a clock to the debugger. Communication can then take place.

0 件の賞賛
返信