Using usbdm library in custom projects

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using usbdm library in custom projects

3,242件の閲覧回数
yarik111475
Contributor II

Hello everyine.

English is not my native lang., so I excuse for any mistakes.

The problem is that. I try to use the usbdm.4.dll library in custom programming project for read/write mcu HCS08 series (I programming in C#).

Now I can read device, but just have not idea how to write device's memory to using this library.

Maybe someone has some custom working project using that .dll (they may be on C or C++, I can understand them).

Thanks.

ラベル(1)
4 返答(返信)

2,864件の閲覧回数
kef2
Senior Contributor V

I'm not familiar with usbdm and your USB<->BDM adapter, but since you can read S08, you also should be able to read write to RAM of your S08 device. Writing to flash memory should be done according to your S08 device flash memory programming algorithm. You can directly manipulate flash module register from BDM, so next step would be to read your S08 datasheet and read about flash module clock initialization and flash erase and program algorithm, which is not the same for all S08 devices.

Regards,

Edward

2,864件の閲覧回数
yarik111475
Contributor II

Thanks, Edward.

Yes, now I can read device (I'm working with GB60 MCU), using C# wrapper for usbdm library from the usbdm project of pgo. But example (here the link: http://usbdm.sourceforge.net/USBDM_V4.12/USBDM_CF_JMxx/html/usbdm_programming.html#USBDM)

is very simple and there is not example of using that library for erase and write MCU. I try to read datasheet, but can not understand how to use that library... If I can see any simple example for using that library, it can be easy for me in my project.

0 件の賞賛
返信

2,864件の閲覧回数
kef2
Senior Contributor V

Looks like there's more suitable place for questions regarding USBDM API

OSBDM and TBDML

Programming with the USBDM API

I think that looking there you should find some examples.

Regards

Edward

0 件の賞賛
返信

2,864件の閲覧回数
yarik111475
Contributor II

Thanks Edward, I'll try to ask developer of that library (pgo) over there. May be he will help me with some source code files...

0 件の賞賛
返信