Using a Chip Antenna & AN2731

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using a Chip Antenna & AN2731

2,285 Views
mjcoury
Contributor I
Hello All -

not to dig [this] post from out of the grave... but  I am also intrested in using a Chip Antenna for an ultra small footprint Zigbee PCB.  I have looked into the AN2731 and frankly there is not much content in that note in re: Chip Antenas.  Nothing speaks to the support ICs that are required to make a chip antenna work or how to tune it nor is there a simple example schematic.  I am just getting into Antenna Theory and I would like some direction before I lay a board out and send it to fab.

Thanks

Message Edited by mjcoury on 2007-05-0108:45 PM

--
Alban Edit: link fixed as pointed to deleted double post.

Message Edited by Alban on 2007-05-01 10:52 PM

Labels (1)
0 Kudos
Reply
1 Reply

1,209 Views
bigmac
Specialist III
Hello,
 
The chip antenna interface requirements will be dictated by the manufacturer of the specific device that you intend using - you won't necessarily be able to generalise.
 
However, it is possible that some devices would be intended to interface with an unbalanced source matched to nominal 50 ohm.  In these cases, it is possible that a matching network will be required, similar to that needed for a resonant "whip" antenna.  No additional "support ICs" should be necessary - matching networks are usually passive.
 
Regards,
Mac
 
 
0 Kudos
Reply