USBMULTILINKBDM to a PCB BDM Header - ¿Any Layout/Pinout?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USBMULTILINKBDM to a PCB BDM Header - ¿Any Layout/Pinout?

跳至解决方案
2,876 次查看
Betadine
Contributor III

Hi.

I´m like more than 1 hour trying to figure out the footprint for the BDM Header for a JM32 MCU.

It´s a very Newbie Question.

 

If I´m considering to buy the 99$ ... USBMULTILINK for only programming my MCU. Then I need a 6 pin header for which the MCU's DS says:

 

!RESET

VDD

GND

BKGD/MS

 

this signals must be connected, ok.

 

USBMULTILINK says about the connector

 

BGND -  1       2 -  GND

      NC - 3        4 - RESET

      NC - 5        6 - VDD

 

Then... I suppose that BGND is BKGD? cause it seems like a GroundB

mmmm it says RESET, and the DS says "!RESET" (inverted) ¿is MULTILINK lying?

 

Ok if this is true, how I make the footprint?

Ive searched a lot but I dont find any more info about this.

 

Dimensions? Pin width? ... something?

 

Regards.

 

Cristian.

标签 (1)
0 项奖励
回复
1 解答
2,258 次查看
celsoken
Contributor V

Dear Betadine,

 

In order to attach to Multilink BDM for JM32 you need a 2x3 std 100 mils male pinhead in your PCB. It's the cheapest pinhead you can find.

The pinout is like you said and the signals are straight connected to the uC pins: VDD, GND/VSS, BKGD and /RESET.

 

I hope it helps.

Cheers,

Celso

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,259 次查看
celsoken
Contributor V

Dear Betadine,

 

In order to attach to Multilink BDM for JM32 you need a 2x3 std 100 mils male pinhead in your PCB. It's the cheapest pinhead you can find.

The pinout is like you said and the signals are straight connected to the uC pins: VDD, GND/VSS, BKGD and /RESET.

 

I hope it helps.

Cheers,

Celso

0 项奖励
回复
2,258 次查看
Betadine
Contributor III

Thank you!

0 项奖励
回复