USBMULTILINKBDM to a PCB BDM Header - ¿Any Layout/Pinout?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USBMULTILINKBDM to a PCB BDM Header - ¿Any Layout/Pinout?

ソリューションへジャンプ
2,906件の閲覧回数
Betadine
Contributor III

Hi.

I´m like more than 1 hour trying to figure out the footprint for the BDM Header for a JM32 MCU.

It´s a very Newbie Question.

 

If I´m considering to buy the 99$ ... USBMULTILINK for only programming my MCU. Then I need a 6 pin header for which the MCU's DS says:

 

!RESET

VDD

GND

BKGD/MS

 

this signals must be connected, ok.

 

USBMULTILINK says about the connector

 

BGND -  1       2 -  GND

      NC - 3        4 - RESET

      NC - 5        6 - VDD

 

Then... I suppose that BGND is BKGD? cause it seems like a GroundB

mmmm it says RESET, and the DS says "!RESET" (inverted) ¿is MULTILINK lying?

 

Ok if this is true, how I make the footprint?

Ive searched a lot but I dont find any more info about this.

 

Dimensions? Pin width? ... something?

 

Regards.

 

Cristian.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,288件の閲覧回数
celsoken
Contributor V

Dear Betadine,

 

In order to attach to Multilink BDM for JM32 you need a 2x3 std 100 mils male pinhead in your PCB. It's the cheapest pinhead you can find.

The pinout is like you said and the signals are straight connected to the uC pins: VDD, GND/VSS, BKGD and /RESET.

 

I hope it helps.

Cheers,

Celso

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,289件の閲覧回数
celsoken
Contributor V

Dear Betadine,

 

In order to attach to Multilink BDM for JM32 you need a 2x3 std 100 mils male pinhead in your PCB. It's the cheapest pinhead you can find.

The pinout is like you said and the signals are straight connected to the uC pins: VDD, GND/VSS, BKGD and /RESET.

 

I hope it helps.

Cheers,

Celso

0 件の賞賛
返信
2,288件の閲覧回数
Betadine
Contributor III

Thank you!

0 件の賞賛
返信