USBMULTILINKBDM to a PCB BDM Header - ¿Any Layout/Pinout?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USBMULTILINKBDM to a PCB BDM Header - ¿Any Layout/Pinout?

Jump to solution
2,867 Views
Betadine
Contributor III

Hi.

I´m like more than 1 hour trying to figure out the footprint for the BDM Header for a JM32 MCU.

It´s a very Newbie Question.

 

If I´m considering to buy the 99$ ... USBMULTILINK for only programming my MCU. Then I need a 6 pin header for which the MCU's DS says:

 

!RESET

VDD

GND

BKGD/MS

 

this signals must be connected, ok.

 

USBMULTILINK says about the connector

 

BGND -  1       2 -  GND

      NC - 3        4 - RESET

      NC - 5        6 - VDD

 

Then... I suppose that BGND is BKGD? cause it seems like a GroundB

mmmm it says RESET, and the DS says "!RESET" (inverted) ¿is MULTILINK lying?

 

Ok if this is true, how I make the footprint?

Ive searched a lot but I dont find any more info about this.

 

Dimensions? Pin width? ... something?

 

Regards.

 

Cristian.

Labels (1)
0 Kudos
Reply
1 Solution
2,249 Views
celsoken
Contributor V

Dear Betadine,

 

In order to attach to Multilink BDM for JM32 you need a 2x3 std 100 mils male pinhead in your PCB. It's the cheapest pinhead you can find.

The pinout is like you said and the signals are straight connected to the uC pins: VDD, GND/VSS, BKGD and /RESET.

 

I hope it helps.

Cheers,

Celso

View solution in original post

0 Kudos
Reply
2 Replies
2,250 Views
celsoken
Contributor V

Dear Betadine,

 

In order to attach to Multilink BDM for JM32 you need a 2x3 std 100 mils male pinhead in your PCB. It's the cheapest pinhead you can find.

The pinout is like you said and the signals are straight connected to the uC pins: VDD, GND/VSS, BKGD and /RESET.

 

I hope it helps.

Cheers,

Celso

0 Kudos
Reply
2,249 Views
Betadine
Contributor III

Thank you!

0 Kudos
Reply