USB time

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决
2,484 次查看
CCandido
Contributor V

Helo,

     
                        for(i=0;i<10;i++)   // send  10 frame

                 {
                
                        EP2_Buffer[0] =3;
                        EP2_Buffer[1] = i;
                        EP2_Buffer[2] =0xAA;
                        
                       EndPoint_IN(EP2,64);     <----------- error not send  10 frame

 

                 while( wait send frame....how do ?) <-------- what BIT  ( CheckEndPoint___IN  )     


                      PTBD^=0x30;                       <----- test see error
                }
  

solution....

 

  EndPoint_IN(EP2,64);    

 

   while( wait send frame )

 

next frame....loop

 

 

 

 

 

 

how do   CheckEndPoint___IN  ( what it bit in bitmap all usb )

 

if not check not send all frames....

 

thanks,

Carlos,

标签 (1)
0 项奖励
回复
1 解答
2,132 次查看
CCandido
Contributor V

hi,

 

 for(c=0;c<10;c++){  send 10 = 10 not failure
                       
                       EP2_Buffer[0] =3;
                       EP2_Buffer[1] =c;
                       EP2_Buffer[2] =0xAA;


                        while(  CheckEndPointIN2(  ));   checking = ok  ,now runinng


                       EndPoint_IN(EP2,64);           
                             PTBD^=0x30;
                                                                    NOTE time interval = 15ms  ( descriptor = 0 interval )
          
                       }

//----------------------------------------------------------------------------------------

UINT8 CheckEndPointIN2( void )
{
 
  if(! EP2_Set.Stat.McuCtlBit.OWN)
   return 0;
   return 1;

}

//--------------------------------------------------------------------------------------------

packet bytes = interval 15ms

decreasing the time of 15 ms?

 

Tsuneo thanks,

 

Carlos,

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,132 次查看
Tsuneo
Contributor IV

> how do   CheckEndPoint___IN  ( what it bit in bitmap all usb )

Check the OWN bit of the BD (Buffer Descriptor) for the target IN endpoint.
On your code, EndPoint_IN() should set this bit to 1, when it passes the endpoint buffer to the SIE. When the SIE completes IN transaction, the OWN bit drops by the SIE.
Therefore, by polling this bit for the transition from 1 to 0, you know the completion of the transaction.

OR
- Poll TOKDNEF bit of INTSTAT. This bit raises when a transaction completes on one of endpoints.
- STAT register points the target endpoint, when a transaction finishes on this endpoint.
This method fits better for process by  hardware interrupt, rather than polling.

The real code depends on the way how the stack declares BD.
Usually, stacks have a macro or a function to do this job.

What is the example, on which you are working?

Tsuneo

0 项奖励
回复
2,133 次查看
CCandido
Contributor V

hi,

 

 for(c=0;c<10;c++){  send 10 = 10 not failure
                       
                       EP2_Buffer[0] =3;
                       EP2_Buffer[1] =c;
                       EP2_Buffer[2] =0xAA;


                        while(  CheckEndPointIN2(  ));   checking = ok  ,now runinng


                       EndPoint_IN(EP2,64);           
                             PTBD^=0x30;
                                                                    NOTE time interval = 15ms  ( descriptor = 0 interval )
          
                       }

//----------------------------------------------------------------------------------------

UINT8 CheckEndPointIN2( void )
{
 
  if(! EP2_Set.Stat.McuCtlBit.OWN)
   return 0;
   return 1;

}

//--------------------------------------------------------------------------------------------

packet bytes = interval 15ms

decreasing the time of 15 ms?

 

Tsuneo thanks,

 

Carlos,

 

0 项奖励
回复