TJA10152IT/5 no signal on RXD pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TJA10152IT/5 no signal on RXD pin

1,267件の閲覧回数
yangwenyou
Contributor I

We have TJA1052IT/5 used on the board to connect a radar sensor, there is a signal detected on CANH and CANL, but no signal on CANRXD pin. Is there something wrong or missed?

タグ(1)
0 件の賞賛
返信
1 返信

1,194件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi,

Make sure that the TJA1052IT is set to normal mode.

The Normal Mode is entered setting pin STB to LOW. In Normal Mode Pin RXD reflects the normal CAN Receiver.


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信