TJA10152IT/5 no signal on RXD pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA10152IT/5 no signal on RXD pin

1,257 Views
yangwenyou
Contributor I

We have TJA1052IT/5 used on the board to connect a radar sensor, there is a signal detected on CANH and CANL, but no signal on CANRXD pin. Is there something wrong or missed?

Tags (1)
0 Kudos
Reply
1 Reply

1,184 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

Make sure that the TJA1052IT is set to normal mode.

The Normal Mode is entered setting pin STB to LOW. In Normal Mode Pin RXD reflects the normal CAN Receiver.


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply