TJA10152IT/5 no signal on RXD pin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TJA10152IT/5 no signal on RXD pin

1,256 次查看
yangwenyou
Contributor I

We have TJA1052IT/5 used on the board to connect a radar sensor, there is a signal detected on CANH and CANL, but no signal on CANRXD pin. Is there something wrong or missed?

标记 (1)
0 项奖励
回复
1 回复

1,183 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi,

Make sure that the TJA1052IT is set to normal mode.

The Normal Mode is entered setting pin STB to LOW. In Normal Mode Pin RXD reflects the normal CAN Receiver.


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复