Supply voltage for read operation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Supply voltage for read operation

1,254件の閲覧回数
rob
Contributor I

I'm using an MC9S08LC60 HCS08 family device. I found the following specification about supply voltage for read operation:

 

0 < Fbus < 8MHz           ----     Vread 1,8 to 3,6V

0 < Fbus < 20MHz         ----     Vread 2,08 to 3,6V

 

Where is the difference? If I use an 8Mhz external resonator to obtain an internal 2Mhz bus clock which voltage range must  I consider? 

 

Thank you

ラベル(1)
0 件の賞賛
返信
1 返信

1,184件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Roberto 

Let me put it in other words.

The minimum voltage level that you need to read the flash at 8 MHz of bus clock is 1.8 V

The minimum voltage level that you need to read the flash at 20 MHz of bus clock is 2.08 V

I hope this will help you.

Regards

Vicente Gomez

0 件の賞賛
返信