Supply voltage for read operation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Supply voltage for read operation

1,223 次查看
rob
Contributor I

I'm using an MC9S08LC60 HCS08 family device. I found the following specification about supply voltage for read operation:

 

0 < Fbus < 8MHz           ----     Vread 1,8 to 3,6V

0 < Fbus < 20MHz         ----     Vread 2,08 to 3,6V

 

Where is the difference? If I use an 8Mhz external resonator to obtain an internal 2Mhz bus clock which voltage range must  I consider? 

 

Thank you

标签 (1)
0 项奖励
回复
1 回复

1,153 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Roberto 

Let me put it in other words.

The minimum voltage level that you need to read the flash at 8 MHz of bus clock is 1.8 V

The minimum voltage level that you need to read the flash at 20 MHz of bus clock is 2.08 V

I hope this will help you.

Regards

Vicente Gomez

0 项奖励
回复