Software compare only in SH4/8 Is it possible?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Software compare only in SH4/8 Is it possible?

Jump to solution
2,463 Views
Leo_Junin
Contributor I

I want to know if the SH series can use "software compare only" although not listed in the reference manual, i.e. MSxB Setting Up: MSxA -> 0:1 and ELSxB: ELSxA -> 0:0.

In the QG series this option is available, and years ago I used the QY series which in the first edition of the reference manual did not include this option and then included in future releases.
I programmed the microprocessor to date of manufacture old and worked wonders. I mean?

 

I hope you understand my bad English.

Thanks, Leo from Argentina

Labels (1)
0 Kudos
Reply
1 Solution
2,105 Views
bigmac
Specialist III

Hello Leo from Argentina,

 

The settings that you describe should provide software only output compare.  This would seem to be an omission from the datasheet.

 

Regards,

Mac from Australia

 

View solution in original post

0 Kudos
Reply
2 Replies
2,106 Views
bigmac
Specialist III

Hello Leo from Argentina,

 

The settings that you describe should provide software only output compare.  This would seem to be an omission from the datasheet.

 

Regards,

Mac from Australia

 

0 Kudos
Reply
2,105 Views
Leo_Junin
Contributor I

Thank you very much, Mac, and figured it was but I could not prove it yet. I happen to be doing development for a company and asked me to used this chip as it is used in other devices.

Thank you very much again.

Leo

0 Kudos
Reply