Software compare only in SH4/8 Is it possible?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Software compare only in SH4/8 Is it possible?

ソリューションへジャンプ
2,535件の閲覧回数
Leo_Junin
Contributor I

I want to know if the SH series can use "software compare only" although not listed in the reference manual, i.e. MSxB Setting Up: MSxA -> 0:1 and ELSxB: ELSxA -> 0:0.

In the QG series this option is available, and years ago I used the QY series which in the first edition of the reference manual did not include this option and then included in future releases.
I programmed the microprocessor to date of manufacture old and worked wonders. I mean?

 

I hope you understand my bad English.

Thanks, Leo from Argentina

ラベル(1)
0 件の賞賛
返信
1 解決策
2,177件の閲覧回数
bigmac
Specialist III

Hello Leo from Argentina,

 

The settings that you describe should provide software only output compare.  This would seem to be an omission from the datasheet.

 

Regards,

Mac from Australia

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,177件の閲覧回数
bigmac
Specialist III

Hello Leo from Argentina,

 

The settings that you describe should provide software only output compare.  This would seem to be an omission from the datasheet.

 

Regards,

Mac from Australia

 

0 件の賞賛
返信
2,177件の閲覧回数
Leo_Junin
Contributor I

Thank you very much, Mac, and figured it was but I could not prove it yet. I happen to be doing development for a company and asked me to used this chip as it is used in other devices.

Thank you very much again.

Leo

0 件の賞賛
返信