Software SPI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Software SPI

5,045 次查看
mjcoury
Contributor I

I need to acess a device using SPI with the Zigbee modules, this of course is an issue becuase the lines are nor broguht out. I searched the forum for software spi which yielded this...

http://forums.freescale.com/freescale/board/message?board.id=8BITCOMM&message.id=15&query.id=2514#M1...

which may or may not help... I have to dig some, but does anyone have any links or resources for setting up a software SPI port.... the zigbee module would be the master and the device is the slave..

thanks

 

(Alban linked)

Message Edited by Alban on 2006-08-10 04:44 PM

标签 (1)
0 项奖励
回复
2 回复数

1,440 次查看
peg
Senior Contributor IV
0 项奖励
回复

1,440 次查看
Alban
Senior Contributor II

Hi Peg,

I see you're an expert in the documentation :smileysurprised:
You should apply for a job in Technical Publications !

Cheers,
Alban.

0 项奖励
回复