Software SPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Software SPI

5,062 Views
mjcoury
Contributor I

I need to acess a device using SPI with the Zigbee modules, this of course is an issue becuase the lines are nor broguht out. I searched the forum for software spi which yielded this...

http://forums.freescale.com/freescale/board/message?board.id=8BITCOMM&message.id=15&query.id=2514#M1...

which may or may not help... I have to dig some, but does anyone have any links or resources for setting up a software SPI port.... the zigbee module would be the master and the device is the slave..

thanks

 

(Alban linked)

Message Edited by Alban on 2006-08-10 04:44 PM

Labels (1)
0 Kudos
Reply
2 Replies

1,457 Views
Alban
Senior Contributor II

Hi Peg,

I see you're an expert in the documentation :smileysurprised:
You should apply for a job in Technical Publications !

Cheers,
Alban.

0 Kudos
Reply