Single Board Computer with the HCS08

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Single Board Computer with the HCS08

3,255 次查看
FC
Contributor III
Hello,
 
I am need of a single board computer with an HCS08 MCU that is ready to be used in the end application.  Are there any companies that produce them?
 
Thanks
标签 (1)
0 项奖励
回复
2 回复数

1,518 次查看
glork
Contributor I
Hello FC.
I have a small company that produces a board based on the MC9S08GB60 (HCS08). It can be had either "bare-bones" or pre-configured with some buffered I/O. It also has an RS-232 port and on-board regulator, etc.
Go to http://gadgetwerksinc.com for a picture and details. Freescale forum members get an un-official 20% discount off the list price.
ron
0 项奖励
回复

1,518 次查看
Jaux
Contributor I

We have developed a simple single-board MCU based on the MC9SAW60CFUE

Features:

. Integrated switching supply, 9-20 VAC input
. AW60 is 5V based
. 24-key keyboard interface ( 8 KBI x 3 scan, active low )
. LCD interface
. RS-485 interface
. All of the GPIO pins are routed to edge pin connectors
. BDM Interface

As a fanatic Freescale junkie, and because you have a small company ( we were all small once), I will let you have the schematics, Gerbers, etc. which you will need to construct the board free of charge.

I am in a good mood, and is Xmas anyway - I will even let you have a blank PCB which you can use to construct the MCU.

See pics attached.

Let me know if you want it.

John Ulyate

RIMG0004.jpg

RIMG0005.jpg

Message Edited by t.dowe on 2009-10-20 01:37 PM
0 项奖励
回复