Simple usb dll and VS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Simple usb dll and VS

2,443件の閲覧回数
Juls
Contributor III

Hi

I have made a cdc device work well

but not its time to move to completly usb

Im using a JM60 and im under windows 7 X64 and vs2010

 

I did listen to How to make a graphical user interface (GUI) for USB communication training twice

My vs project is in CLR (way more easier to build gui)

and at the part to drag the dll into the tool box I get a bug

placing it work but trying to place the simple usb into my form throw and error about LFSwinusb.dll in vs install directory (that file doesnt exist. and the object is not created :smileyfrustrated:

 

Anyone made that work?

Thanks

 

Ive also spend 2-3 hours trying to make winusb work but im not able to make all that compile

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,783件の閲覧回数
Tsuneo
Contributor IV

In this topic, it was discussed once.

SimpleUSB & Windows 7
https://community.freescale.com/thread/80364

Tsuneo

0 件の賞賛
返信

1,783件の閲覧回数
Juls
Contributor III

Hi

I have read it

im using C++ now C#

and I couldn t get it to compile

 

But now it work (have tried a device yet)

had to run vs in admin to add the simple usb dll component then i could use it as a user

0 件の賞賛
返信