Simple string assignment problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Simple string assignment problem

1,477件の閲覧回数
protoease
Fresh Out Contributor

Banging my head against the wall on the following simple character string assignment problem:

 

char user_text[6];

 

// somewhere else in code:

user_text[] = {"text"};

 

Compiler throws up alarm on C1830: Modifiable lvalue expected.

 

What am I doing wrong?

 

I don't want to include string support as I can't support the burden size-wise.

 

Appreciate any help, I'm sure it is something silly and simple.

 

Thanks,

Aaron

ラベル(1)
0 件の賞賛
返信
1 返信

1,188件の閲覧回数
bigmac
Specialist III

Hello Aaron,

 

Your string assignment is not allowable in C.  With this format, a constant or variable may only be initialised, i.e. at the same time the constant or variable is defined.

 

To assign data to an array variable within a function, each element of the array woulld need to be individually written.

user_text[0] = 't';

user_text[1] = 'e';

user_text[2] = 'x';

user_text[3] = 't';

user_text[4] = 0;

 

To copy constant string data into the array variable, you will need to write your own function if you do not wish to include an existing library within your project.  Keep in mind that only the code size associated with the particular library functions that you use, will be added to your project.

 

Regards,

Mac

0 件の賞賛
返信