Seial Bootloader for MC9S08AC16

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Seial Bootloader for MC9S08AC16

1,590件の閲覧回数
willyrey
Contributor I

Hello

We are using the universal bootloader from AN2295, Version 10.0.13.0. On the device MC9S08AC16 we are using the bootloader ASM Software from the very same AN2295 package. The device could be programmed well. Connecting to master Software we got the results as seen on the attached screenshot. It seems that the slave Software could not trim the busfrequency correct. the transmitted value of 0xB1 is away from 0xFC as required. We have a Resonator of 6.000 MHz on the board, so could we use this frequency instead, without selftrimming? Thank you vers much for your Support.

Best regards, Willy

ラベル(1)
0 件の賞賛
返信
0 返答(返信)