Seial Bootloader for MC9S08AC16

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Seial Bootloader for MC9S08AC16

1,598 Views
willyrey
Contributor I

Hello

We are using the universal bootloader from AN2295, Version 10.0.13.0. On the device MC9S08AC16 we are using the bootloader ASM Software from the very same AN2295 package. The device could be programmed well. Connecting to master Software we got the results as seen on the attached screenshot. It seems that the slave Software could not trim the busfrequency correct. the transmitted value of 0xB1 is away from 0xFC as required. We have a Resonator of 6.000 MHz on the board, so could we use this frequency instead, without selftrimming? Thank you vers much for your Support.

Best regards, Willy

Labels (1)
0 Kudos
Reply
0 Replies