Secure device erased. Do you wish t...

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Secure device erased. Do you wish t...

4,163件の閲覧回数
employee
Contributor I
Hi,     I would like to send you my problem with erasing of Flash memory MCU. 1. I erased memory and communication with MCU was shuting down during erasing. 2. When I did erasing again I was get the message: Sorry for my english. Thank you very much for your answers. Petr



Message Edited by employee on 2007-08-13 07:11 PM

 

doc11.doc

Message Edited by t.dowe on 2009-10-27 02:00 PM
ラベル(1)
0 件の賞賛
返信
5 返答(返信)

1,971件の閲覧回数
employee
Contributor I
Problem is resolved. The pins 15-16 was interconnected.MCU is OK. MCU was erased and programmed.
 
Petr
0 件の賞賛
返信

1,971件の閲覧回数
peg
Senior Contributor IV
Hi employee,
 
Aside from the shutting down, this is normal.
What happens after you click Yes?
 
0 件の賞賛
返信

1,971件の閲覧回数
employee
Contributor I
When I press Yes, the programming algorithm was only reloaded. The MCU Flash memory wasn't erasing.
 
Thank you very much.
 
 
Petr
0 件の賞賛
返信

1,971件の閲覧回数
peg
Senior Contributor IV
Hi again,
 
The Blank check fails? What is the message?
 
Do a Upload Module and what do you get? Just a one line s19 file or a very big one?
 
 
0 件の賞賛
返信

1,971件の閲覧回数
employee
Contributor I
Hi,
I'm going to answer afternoon when I will arrive from work. I'm going to send printscreens during erasing and programming. I have the other MCU and this MCU is OK for the same program modul.
 
Thanks.
 
Petr
0 件の賞賛
返信