SMAC based boards compatibility

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SMAC based boards compatibility

1,863件の閲覧回数
multipoda
Contributor I
Hi, I designed a 12313-SRB based prototype and I have a 13192-SARD too.
 
Using SMAC 4.1a protocol, ¿Are they compatibles? ¿Can I use SMAC 4.1a in one board and SMAC 4.1c in the other?
 
I mean, I need a 13912-SARD  receiver because it have a RS232 port and a small size, and all the transmiters are 12313-SRB reference design based boards.
 
Thanks in advance.
ラベル(1)
0 件の賞賛
返信
1 返信

1,074件の閲覧回数
NLFSJ
Contributor III
Hi,
 
Yes, as long as the feature set is common.  In some of the newer versions, we have added features such as repeaters, security, etc.
 
Also, the latest SMAC included with our BeeKit is 4.2
 
 
Regards,
Nina
0 件の賞賛
返信