SMAC based boards compatibility

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SMAC based boards compatibility

1,870 Views
multipoda
Contributor I
Hi, I designed a 12313-SRB based prototype and I have a 13192-SARD too.
 
Using SMAC 4.1a protocol, ¿Are they compatibles? ¿Can I use SMAC 4.1a in one board and SMAC 4.1c in the other?
 
I mean, I need a 13912-SARD  receiver because it have a RS232 port and a small size, and all the transmiters are 12313-SRB reference design based boards.
 
Thanks in advance.
Labels (1)
0 Kudos
Reply
1 Reply

1,081 Views
NLFSJ
Contributor III
Hi,
 
Yes, as long as the feature set is common.  In some of the newer versions, we have added features such as repeaters, security, etc.
 
Also, the latest SMAC included with our BeeKit is 4.2
 
 
Regards,
Nina
0 Kudos
Reply