SCI and UART mean the same?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SCI and UART mean the same?

15,616 次查看
treasure
Contributor I

Thanks!

标签 (1)
0 项奖励
回复
4 回复数

11,374 次查看
Lundin
Senior Contributor IV
Yeah it is exactly the same thing. Semiconductor manufacturers name things differently, mainly because of old stubborn arrogance. Motorola/Freescale likely named it SCI because they wouldn't give credit to the name UART, which is heavily asociated with National Semi. Similarly, you will often find Freescale's competition call SPI for "serial synchronous something", as they won't give Motorola credit for inventing it.
0 项奖励
回复

10,217 次查看
Fast
Contributor IV

Well Eric Hackett at TI said about LIN bus "Serial Communication Principles
The previously-mentioned SCI is the dominant interface used between LIN transceivers and the
microcontrollers that communicate with them. UART was used originally, but fault-free interface via UART
is known to be difficult to achieve." Is that just about detecting Sync Break? HW that got added to early SCI implimentations to specifically aid LIN support. Oh and IR transmission support with short pulses, probably continues to to types with no A in UART that use a clock and start to feel like SPI.

0 项奖励
回复

11,374 次查看
peg
Senior Contributor IV

Hello,

 

As far as Freescale 8 bit goes, an SCI (Serial Communications Interface) includes a UART (and not much else). So essentially they are one and the same.

 

0 项奖励
回复

10,019 次查看
thetopnxp
Contributor I

Thank you! ) I used different semiconductor-based components to create a device for generating high-quality images. Now I realize that I could have saved a lot of money on components. But I will know for the future ))

0 项奖励
回复