SCI and ESCI difference

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SCI and ESCI difference

3,655件の閲覧回数
periklis
Contributor I
What is the difference between SCI and ESCI ?
I have an application for 908KX8CP but now that it has come to the end of its life i need to replace it with an other MCU. I want to know if 908QB8 is suitable. In my application i use SCI and the operation is 5V.
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,566件の閲覧回数
bigmac
Specialist III
Hello,
 
ESCI actually means enhanced SCI, so there should be no problems to operate as a normal SCI.  I believe the enhancement actually refers to the optional ability to handle LIN protocol for automotive use, and the provision of a baud rate prescaler that allows fine adjustment of baud rate.  There is also an "arbiter" facility for measurement of incoming bit period.
 
These additional facilities don't have to be used if you don't wish to.
 
Regards,
Mac
 
0 件の賞賛
返信

1,566件の閲覧回数
joerg
Contributor II
Hi periklis
The difference between a SCI and a ESCI block is that ESCI has some enhancements like the name implies. This means, that with a ESCI you can do all the SCI stuff AND ie. baudrate recognition and adjustment etc. So the QB8 could meet your needs.

Saluti Joerg
0 件の賞賛
返信