S908QC16E0MDTER RAM check

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S908QC16E0MDTER RAM check

1,398件の閲覧回数
王剑翰
Contributor III

Dear,

 

We use the CANalyzer tool to test the failure board and find the defect is for SUB RAM CHECK. (The failure only occurs in high temperature(105℃))

So I want to check the unit(S908QC16E0MDTER is as the sub cpu in the board) and check the error address information, but I don't know how to do it.

 

Can you recommend a software tool  or debug program] for this case to check the error address information of RAM?

 

Thank you~!

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,286件の閲覧回数
Rick_Li
NXP Employee
NXP Employee

Hi, my suggestion is using classic CodeWarrior v6.3 from Freescale or CPROG08SZ from PEmicro.

CodeWarrior:

CodeWarrior for Microcontrollers (Classic IDE|Freescale

CPROG08SZ:

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=12

as to the debugger interface, a cyclonePro or USB-ML-MON08 is needed.

see them at:

P&E Microcomputer Systems

0 件の賞賛
返信

1,286件の閲覧回数
王剑翰
Contributor III

Thank you for your kindly answer.

I have get the tools: CPROG08SZ from PEmicro and USB-ML-MON08.

Then, how to use them to check the error address information of RAM? Could you kindly give me an example ?

Best regards!

0 件の賞賛
返信