S908QC16E0MDTER RAM check

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S908QC16E0MDTER RAM check

1,438 Views
王剑翰
Contributor III

Dear,

 

We use the CANalyzer tool to test the failure board and find the defect is for SUB RAM CHECK. (The failure only occurs in high temperature(105℃))

So I want to check the unit(S908QC16E0MDTER is as the sub cpu in the board) and check the error address information, but I don't know how to do it.

 

Can you recommend a software tool  or debug program] for this case to check the error address information of RAM?

 

Thank you~!

Labels (1)
0 Kudos
Reply
2 Replies

1,326 Views
Rick_Li
NXP Employee
NXP Employee

Hi, my suggestion is using classic CodeWarrior v6.3 from Freescale or CPROG08SZ from PEmicro.

CodeWarrior:

CodeWarrior for Microcontrollers (Classic IDE|Freescale

CPROG08SZ:

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=12

as to the debugger interface, a cyclonePro or USB-ML-MON08 is needed.

see them at:

P&E Microcomputer Systems

0 Kudos
Reply

1,326 Views
王剑翰
Contributor III

Thank you for your kindly answer.

I have get the tools: CPROG08SZ from PEmicro and USB-ML-MON08.

Then, how to use them to check the error address information of RAM? Could you kindly give me an example ?

Best regards!

0 Kudos
Reply