S08QE8 with External Oscillator

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S08QE8 with External Oscillator

1,783 Views
MatthewScott_DE
Contributor II

I am designing with the 16 pin S08QE8 and plan to use an external oscillator (not a crystal or resonator).  Do I drive the EXTAL pin with the oscillator output and leave the XTAL pin hanging or is there another setup that should be used?

 

Thank you very much for your time

Labels (1)
0 Kudos
Reply
4 Replies

1,645 Views
MatthewScott_DE
Contributor II

Thank you both very much

0 Kudos
Reply

1,645 Views
rocco
Senior Contributor II

Hi Matthew Scott,

 

Welcome to the forum.


Do I drive the EXTAL pin with the oscillator output and leave the XTAL pin hanging?

Yes.

 

0 Kudos
Reply

1,645 Views
bigmac
Specialist III

Hello,

 

An additional consideration may be, that if ICSC2_EREFS bit is set to zero, the XTAL pin should be available as GPIO.

 

Regards,

Mac

 

0 Kudos
Reply

1,645 Views
rocco
Senior Contributor II

bigmac wrote:

An additional consideration may be, that if ICSC2_EREFS bit is set to zero, the XTAL pin should be available as GPIO.


Good point. You do not need to "leave it hanging". You can do something useful with it.

0 Kudos
Reply